21.11.16 run_selected_actions
(Ask a Question)Description
FlashPro-specific Tcl command. Runs the selected action on the specified programmer. If no programmer name is specified, the action is run on all connected programmers. A programming file must be loaded.
run_selected_actions [-name "name"] \
                     [-force_rtg4_erase "TRUE | FALSE"] \
                     [-prog_spi_flash "TRUE | FALSE"] \
                     [-disable_prog_design "TRUE | FALSE"] \
                     [-spi_flash_image "spi_flash_image"] \
                     [-spi_flash_action "spi_flash_action"]Arguments
| Parameter | Type | Description | 
|---|---|---|
| name | string | Optional argument that specifies the programmer name. You can repeat this argument for multiple programmers(example below). | 
force_rtg4_erase  | boolean  | This action is for RT4G device only. When the value of this option is set to "TRUE" the erase action will be run on RT4G device when erase action is executed in batch mode using TCL script.  | 
disable_prog_design  | boolean  | Specify 1 or "TRUE" to disable device programming, specify 0 or "FALSE" to enable device programming.  | 
prog_spi_flash  | boolean  | Specify 1 or "TRUE" to enable spi flash programming, sepcify 0 or "FALSE" to disable spi flash programming.  | 
spi_flash_image  | string  | Provide the path of spi flash image (bin) file.  | 
spi_flash_action  | string  | The value can be one of these: PROGRAM_SPI_IMAGE, VERIFY_SPI_IMAGE, READ_SPI_IMAGE, ERASE_SPI_FLASH.  | 
| Return Type | Description | 
|---|---|
| None | None | 
Error Codes
| Error Code | Description | 
|---|---|
| None | The programmer with name doesn't exist. | 
| None | Parameter 'name' has illegal value. | 
| None | Parameter 'argument_name' is not defined. Valid command formatting is 'run_selected_actions [-name "name"]* [-force_rtg4_erase "TRUE | FALSE"] \ [-prog_spi_flash "TRUE | FALSE"] [-disable_prog_design "TRUE | FALSE"] \ [-spi_flash_image "spi_flash_image"] [-spi_flash_action "spi_flash_action"]. | 
Supported Families
| PolarFire® | 
| SmartFusion® 2 | 
IGLOO® 2  | 
| RTG4™ | 
Example
The following example runs the selected actions on the programmers 'FP30085' and 'FP30086':
run_selected_actions -name {FP300085} -name {FP300086}The following example catches pass/fail:
if {[catch {run_selected_actions -name {FP300085}]} {
    puts "Error running Action"
} else {
    puts "Action passed"}The following example returning exit code to the command line (returns exit 99 on script failure, otherwise returns 0):
if {[catch {run_selected_actions}]}{
    exit 99
} else {
    exit 0
}See Also
- set_programming_action