Description
This Tcl command changes the user name of a programmer. Enter the new programmer name in the Programmer window to rename the programmer. By default, the programmer name is the same as the programmer ID.
set_prg_name -name { name } -new_name { new_name }
Arguments
| Parameter | Type | Description | 
|---|
| name | string | Identifies the old programmer name. | 
| new_name | string | Specifies the new programmer name. | 
| Return Type | Description | 
|---|
| None | None | 
Error Codes
| Error Code | Description | 
|---|
| None | Parameter 'param_name' is not defined. Valid command formatting is set_prg_name -name "name" -new_name "new_name" | 
| None | Required parameter 'new_name' is missing. | 
| None | The programmer with name 'some_device_name' does not exist. | 
Example
The following example changes the name of the programmer 'FP300086' to 'FP3Prg2':
set prj_name "FP300086"
set_prg_name -name "$prj_name" -new_name {FP3Prg2}