Description
This TCL command allows the user to select the FlashPro express mode: Operator mode or Developer mode. Operator mode is the current default mode. Developer mode allows to update jobs before running programming.
Note: This TCL command will error out if there is an open job. The user has to close open jobs (or have close_project TCL command in the TCL script) before running this command.
set_fpexpress_mode [-mode {operator|developer}]
Arguments
| Parameter | Type | Description | 
|---|
| mode | string | Specify FlashPro express mode. The possible value for this argument are: - operator_mode - FlashPro Express mode is set to operator mode.
 - developer_mode - FlashPro Express mode is set to developer mode.
 
  | 
| Return Type | Description | 
|---|
| None | None | 
Error Codes
| Error Code | Description | 
|---|
| None | Required parameter 'mode' is missing. | 
| None | Parameter 'param_name' is not defined. Valid command formatting is 'set_fpexpress_mode -mode "operator_mode | developer_mode"'. | 
| None | mode: Invalid argument value: ''(expecting operator_mode or developer_mode). | 
Example
This example sets FlashPro express mode as "developer_mode":
set_fpexpress_mode -mode {developer_mode}