Description
            
            This Tcl command updates all the FlashPro6 programmers that require update. This
                command takes no parameters. To execute the Tcl Command in Libero SoC, add the
                command before run_tool. To execute the Tcl command in FlashPro
                Express tool or SmartDebug tool, add the Tcl command before
                    run_selected_actions.
            update_fp6_programmers
        Arguments
            
            | Parameter | Type | Description | 
|---|
| None | None | None | 
 
            | Return Type | Description | 
|---|
| None | None | 
 
        Error Codes
            
            | Error Code | Description | 
|---|
| None | Parameter 'param_name' is not defined. Valid command formatting
                                is 'update_fp6_programmers'. | 
 
        Example
            
            This example updates all the FlashPro6 programmers that require update.
            update_fp6_programmers