21.11.28 set_spi_flash_file
(Ask a Question)Description
This Tcl command specifies SPI Flash programming file(.bin) to be associated with the device.
set_spi_flash_file [-name {name}] \
-file {path and the name of the programming file} \
-no_fileArguments
| Parameter | Type | Description | 
|---|---|---|
name  | string  | This argument must be specified only in chain programming mode. It is optional.  | 
file  | string  | Specifies the SPI Flash programming file *.bin.  | 
no_file  | none  | Specifies to unload/unspecify the SPI Flash programming file.  | 
| Return Type | Description | 
|---|---|
| None | None | 
Error Codes
| Error Code | Description | 
|---|---|
None  | Required parameter 'action' is missing.  | 
None  | The device with name does not exist.  | 
Supported Families
| PolarFire® | 
| SmartFusion® 2 | 
Example
The following example sets the "VERIFY_SPI_IMAGE" SPI Flash programming action in single programming mode:
set_spi_flash_file -name {MPFS250T_ES} \
                   -spi_flash_action {VERIFY_SPI_IMAGE}