21.11.9 enable_prg
(Ask a Question)Description
This Tcl command enables or disables the programmer specified. It will give error if the programmer specified for the -name option is not connected to that machine.
enable_prg \
-name {programmer_id} \
-enable {value}Arguments
| Parameter | Type | Description | 
|---|---|---|
| name | string | Specify the programmer ID. | 
| enable | boolean | Specify 1 or TRUE to enable the programmer, specify 0 or FALSE to disable the programmer. This is mandatory. | 
| Return Type | Description | 
|---|---|
| None | None | 
Error Codes
| Error Code | Description | 
|---|---|
| None | Programmer mentioned in the -name parameter is not connected to the machine | 
None  | The programmer with name 'programmer ID' does not exist.  | 
None  | Required parameter 'enable' is missing.  | 
None  | Required parameter 'name' is missing.  | 
None  | Parameter 'param_name' is not defined. Valid command formatting is enable_prg [-name "name"]+ -enable "TRUE | FALSE".  | 
Supported Families
| PolarFire® | 
| SmartFusion® 2 | 
Example
The following command enables the programmer with programmer ID 13802A15:
enable_prg -name {13802A15} -enable 1