TCPIP_STACK_NetGetType Function

C

TCPIP_NETWORK_TYPE TCPIP_STACK_NetGetType(
    TCPIP_NET_HANDLE hNet
);

Description

This function returns the network interface type: primary or alias.

Preconditions

The TCP/IP stack should have been initialized by TCPIP_STACK_Initialize() and support for alias interfaces enabled. Otherwise, all interfaces are primary.

Parameters

ParametersDescription
hNetInterface handle.

Returns

  • TCPIP_NETWORK_TYPE_PRIMARY - If interface exists and the interface is a primary interface.
  • TCPIP_NETWORK_TYPE_ALIAS - If the interface exists and is an alias.
  • TCPIP_NETWORK_TYPE_UNKNOWN - No such interface exists.

Remarks

None.