TCPIP_STACK_VersionGet Function
C
unsigned int TCPIP_STACK_VersionGet(
const SYS_MODULE_INDEX index
);
Description
This function gets the TCP/IP stack version. The version is encoded as major * 10000 + minor * 100 + patch. The stringed version can be obtained using TCPIP_STACK_VersionStrGet().
Preconditions
None.
Parameters
Parameters | Description |
---|---|
index | Identifier for the object instance to get the version for. |
Returns
- Current driver version in numerical format.
Remarks
None.
Example
unsigned int version;
version = TCPIP_STACK_VersionGet( TCPIP_STACK_INDEX_1 );
if(version < 110200)
{
// Do Something
}