TCPIP_STACK_HEAP_POOL_ENTRY Structure

C

typedef struct {
uint16_t entrySize;
uint16_t nBlocks;
uint8_t nExpBlks;
} TCPIP_STACK_HEAP_POOL_ENTRY;

Description

Internal pool configuration data.

This data type defines the data required to initialize the TCP/IP stack internal memory pool.

Preconditions

None.

Members

MembersDescription
entrySizeSize of the blocks in this pool entry.
nBlocksNumber of blocks to create for this entry.
nExpBlksNumber of blocks to expand/allocate when an allocation in this entry failed.

Remarks

Pool entries should follow these 2 rules:

  • They should have distincy block sizes: entrySize. Multiple entries having the same entrySize is not supported.
  • Pool entries should have a non-zero block size. Entries with 0 block size are not supported.

If these conditions are not observed, the heap creation will fail. To expand/dynamically allocate at run time the expansionHeapSize needs to be != 0; If nExpBlks == 0, then no allocation will be tried for this particular entry.