TCPIP_STACK_NetDown Function

C

bool TCPIP_STACK_NetDown(
    TCPIP_NET_HANDLE netH
);

Description

This function performs the deinitialization of a net interface. As part of this process, the corresponding MAC driver is deinitialized.

Preconditions

The TCP/IP stack should have been initialized by TCPIP_STACK_Initialize() and the TCPIP_STACK_Status() returned SYS_STATUS_READY. The network interface should be up and running.

Parameters

ParametersDescription
netHInterface handle.

Returns

  • True - If success.
  • False - If no such network interface or the interface is already down.

Remarks

If the interface to be brought down is a primary interface, then all its aliases will be brought down as well. If the interface to be brought down as an alias interface, then other interfaces won't be affected.