TCPIP_STACK_NetIPv6AddressGet Function

C

IPV6_ADDR_HANDLE TCPIP_STACK_NetIPv6AddressGet(
    TCPIP_NET_HANDLE netH, 
    IPV6_ADDR_TYPE addType, 
    IPV6_ADDR_STRUCT* pAddStruct, 
    IPV6_ADDR_HANDLE addHandle
);

Description

This function allows the listing of the IPv6 addresses associated with an interface.

Preconditions

The TCPIP_STACK_Initialize() function must have been called before calling this function. The network interface should be up and running.

Parameters

ParametersDescription
netHInterface handle to set the address of.
addTypeType of address to request. IPV6_ADDR_TYPE_UNICAST and IPV6_ADDR_TYPE_MULTICAST supported for now.
pAddStructStructure provided by the user that will be filled with corresponding IPV6_ADDR_STRUCT data.
addHandleAn address handle that allows iteration across multiple IPv6 addresses. On the first call, it has to be 0; It will begin the listing of the IPv6 addresses. On subsequent calls, it has to be a handle previously returned by a call to this function.

Returns

  • Non-NULL IPV6_ADDR_HANDLE - If a valid IPv6 address was found and the pAddStruct structure was filled with data.
  • 0 - If no such interface or interface is not enabled.

Remarks

None.

Example

IPV6_ADDR_STRUCT currAddr;
IPV6_ADDR_HANDLE currHandle;
TCPIP_NET_HANDLE hNet = TCPIP_STACK_NetHandleGet("PIC32INT");
char    ipv6AddBuff[44];

currHandle = 0;
do
{
    currHandle = TCPIP_STACK_NetIPv6AddressGet(netH, IPV6_ADDR_TYPE_UNICAST, &currAddr, currHandle);
    if(currHandle)
    {   // have a valid address; display it
        TCPIP_HELPER_IPv6AddressToString(&currAddr.address, ipv6AddBuff, sizeof(ipv6AddBuff));
    }
}while(currHandle != 0);