TCPIP_MODULE_SignalGet Function
C
TCPIP_MODULE_SIGNAL TCPIP_MODULE_SignalGet(
TCPIP_STACK_MODULE moduleId
);
Description
This function provides a read only value of the current signals for a stack module.
Preconditions
The TCP/IP stack should have been initialized by TCPIP_STACK_Initialize() and the TCPIP_STACK_Status() returned SYS_STATUS_Ready.
Parameters
Parameters | Description |
---|---|
moduleId | Module ID. |
Returns
- The current value of the module's signals.
Remarks
The signals are processed and cleared inside the stack. It is not possible to clear a signal that's pending using this API.
Example
TCPIP_MODULE_SIGNAL currSIgnal = TCPIP_MODULE_SignalGet(TCPIP_MODULE_HTTP_SERVER);