TCPIP_STACK_EventsPendingGet Function
C
TCPIP_EVENT TCPIP_STACK_EventsPendingGet(
TCPIP_NET_HANDLE hNet
);
Description
This function returns the currently pending events. Multiple events can be ORed together as they accumulate.
Preconditions
The TCP/IP stack should have been initialized by TCPIP_STACK_Initialize() and the TCPIP_STACK_Status() returned SYS_STATUS_READY. The network interface should be up and running.
Parameters
Parameters | Description |
---|---|
hNet | Network handle. |
Returns
- The currently TCP/IP pending events.
Remarks
This is the preferred method to get the current pending stack events. Even with a notification handler in place, it's better to use this function to get the current pending events. The returned value is just a momentary value. The pending events can change any time. If the hNet refers to an alias interface, the events of the primary interface are returned.
Example
TCPIP_EVENT currEvents = TCPIP_STACK_EventsPendingGet( hNet);