TCPIP_STACK_NetBiosNameSet Function

C

bool TCPIP_STACK_NetBiosNameSet(
    TCPIP_NET_HANDLE netH, 
    const char* biosName
);

Description

This function sets the network interface NetBIOS name.

Preconditions

The TCP/IP stack should have been initialized by TCPIP_STACK_Initialize() and the TCPIP_STACK_Status() returned SYS_STATUS_READY. The network interface should be up and running.

Parameters

ParametersDescription
netHInterface handle to set name of.

Returns

  • True - If the NetBIOS name of the interface is set.
  • False - If no such interface or interface is not enabled.

Remarks

Exercise extreme caution when using these functions to change the settings of a running network interface. Changing these parameters at runtime can lead to unexpected behavior or loss of network connectivity. The preferred way to change the parameters for a running interface is to do so as part of the network configuration passed at the stack initialization.

Example

TCPIP_NET_HANDLE netH = TCPIP_STACK_NetHandleGet("PIC32INT");
TCPIP_STACK_NetBiosNameSet(netH, myBiosName);