TCPIP_STACK_NetDefaultGet Function
C
TCPIP_NET_HANDLE TCPIP_STACK_NetDefaultGet();
Description
This function returns the current default network interface in the TCP/IP stack. This is the interface on which packets will be transmitted when the internal routing algorithm cannot detect a match for an outgoing packet.
Preconditions
The TCP/IP stack should have been initialized by TCPIP_STACK_Initialize() and the TCPIP_STACK_Status() returned SYS_STATUS_READY.
Returns
- The default network interface.
Remarks
This function is intended for multi-hoed hosts, with the TCP/IP stack running multiple interfaces.