TCPIP_STACK_HEAP_LastError Function
C
TCPIP_STACK_HEAP_RES TCPIP_STACK_HEAP_LastError(
TCPIP_STACK_HEAP_HANDLE heapH
);
Description
This function returns the last error encountered in a heap operation. It clears the value of the last error variable.
Preconditions
heapH - valid heap handle.
Parameters
Parameters | Description |
---|---|
heapH | Handle to a heap. |
Returns
- The last error encountered in an operation
- TCPIP_STACK_HEAP_RES_OK if no error occurred.
Remarks
The heap holds an error variable storing the last error encountered in an operation. This should be consulted by the caller after each operation that returns an invalid result for checking what the error condition was.