TCPIP_Helper_SecurePortGetByIndex Function

C

uint16_t TCPIP_Helper_SecurePortGetByIndex(
    int index, 
    bool streamSocket, 
    int* pnIndexes
);

Description

This function returns the secure TCP/UDP port situated at the internal port table requested index. It also returns the number of indexes currently in the table.

Preconditions

TCP/IP stack properly initialized.

Parameters

ParametersDescription
indexThe port index to query. 0 should always be a valid index.
streamSocketIf true, a stream/TCP port is queried. Else, a datagram/UDP port is queried.
pnIndexesPointer to store the number of indexes that the table currently has. Could be NULL if not needed.

Returns

  • A port number corresponding to the required index.
  • 0 if the corresponding slot is free or the port is not associated with the requested stream/datagram flag.

Remarks

None.