TCPIP_STACK_NetMulticastGet Function
C
TCPIP_NET_HANDLE TCPIP_STACK_NetMulticastGet();
Description
This function returns the current default multicast network interface in the TCP/IP stack. This is the interface on which IGMP and multicast packets will be transmitted when a default interface is specified.
Preconditions
The TCP/IP stack should have been initialized by TCPIP_STACK_Initialize() and the TCPIP_STACK_Status() returned SYS_STATUS_READY.
Returns
- The fault multicast network interface.
Remarks
This function is intended for a TCP/IP stack implementing IGMP.