TCPIP_Helper_StringToMACAddress Function

C

bool TCPIP_Helper_StringToMACAddress(
    const char* str, 
    uint8_t macAddr[6]
);

Description

This function parses a MAC address string "aa:bb:cc:dd:ee:ff" or "aa-bb-cc-dd-ee-ff" into an hex MAC address.

Preconditions

macAddr - valid pointer to a 6 byte MAC address field.

Parameters

ParametersDescription
strPointer to a colon separated MAC address string.
macAddrPointer to buffer to store the result.

Returns

  • True - A MAC address was successfully decoded.
  • False - No MAC address could be found, of the format was incorrect.

Remarks

If str == NULL or strlen(str) == 0, the result will be address 0.