TCPIP_STACK_NetAddressDnsPrimarySet Function
C
bool TCPIP_STACK_NetAddressDnsPrimarySet(
TCPIP_NET_HANDLE netH,
IPV4_ADDR* ipAddress
);
Description
This function sets the network interface primary IPv4 DNS address.
Preconditions
The TCPIP_STACK_Initialize() function must have been called before calling this function. The network interface should be up and running.
Parameters
Parameters | Description |
---|---|
netH | Interface handle to set the DNS address of. |
ipAddress | IP address to set. |
Returns
- True - If success.
- False - If no such interface or interface is not enabled.
Remarks
Exercise extreme caution when using these functions to change the settings of a running network interface. Chaning these parameters at runtime can lead to unexpected behavior or loss of network connectivity. The preferred way to change the parameters for a running interface is to do so as part of the network configuration passed at the stack initialization.
Example
TCPIP_NET_HANDLE netH = TCPIP_STACK_NetHandleGet("PIC32INT");
TCPIP_STACK_NetAddressDnsPrimarySet(netH, &myIPAddress);