28.2.49 __builtin_return_address
Description
Returns the return address of the current function, or of one of its callers. For the
level argument, a value of 0 yields the return address
of the current function, a value of 1 yields the return address of the caller of the
current function, and so forth. When level exceeds the current stack depth, 0 will be
returned. This function should only be used with a non-zero argument for debugging
purposes.
Prototype
int __builtin_return_address (const int level);
Argument
level – Number of frames to scan up the call stack.
Return Value
Returns the return address of the current function, or of one of its callers.
Assembler Operator/ Machine Instruction
return_address