28.2.1 __builtin_ACCL, __builtin_ACCH, __builtin_ACCU
Description
This function can be used to gain access to the low, high, or upper portion of an accumulator value. For example:
volatile register int value asm(“A”);
int result = __builtin_ACCL(value);
The example result will be the low 16-bits stored in the accumulator which holds
value.
These builtins allow access to the parts of an accumulator in a way that is optimizer safe.
Prototype
int __builtin_ACCL(int value);
int __builtin_ACCH(int value);
int __builtin_ACCU(int value);
Argument
value – Integer number to set accumulator value.
Return Value
Returns the low, high or upper portion of the accumulator.
Assembler Operator/ Machine Instruction
None
Error Messages
None