28.2.61 __builtin_tbladdress
Description
Returns a value that represents the address of an object in program memory. The argument
p must be the address of an object in an EE data, PSV or
executable memory space; otherwise an error message is produced and the compilation
fails. See the space attribute in Variable Attributes.
Prototype
unsigned long __builtin_tbladdress(const void *p);
Argument
p object address
Return Value
Returns an unsigned long value that represents the address of an object
in program memory.
Assembler Operator/ Machine Instruction
tbladdress
Error Messages
The following error message is produced when this function is used incorrectly: “Argument
to __builtin_tbladdress() is not the address of an object in code, psv,
or eedata section”.
The argument must be an explicit object address.
For example, if obj is object in an executable or read-only
section, the following syntax is valid:
unsigned long page = __builtin_tbladdress(&obj);