28.2.63 __builtin_tblpage
Description
Returns the table page number of the object whose address is given as a parameter. The
argument p must be the address of an object in an EE data, PSV
or executable memory space; otherwise an error message is produced and the compilation
fails. See the space attribute in Variable Attributes.
Prototype
unsigned int __builtin_tblpage(const void *p);
Argument
p – object address
Return Value
Returns the table page number of the object whose address is given as a parameter.
Assembler Operator/ Machine Instruction
tblpage
Error Messages
The following error message is produced when this function is used incorrectly: “Argument
to __builtin_tblpage() is not the address of an object in code, psv, or
eedata section.”
The argument must be an explicit object address.
For example, if obj is object in an executable or read-only
section, the following syntax is valid:
unsigned page = __builtin_tblpage(&obj);