28.2.18 __builtin_dmapage
Description
Obtains the page number of a symbol within DMA memory.
For example:
unsigned int result;
char buffer[256] __attribute__((space(dma)));
result = __builtin_dmapage(&buffer);
Might generate:
mov #dmapage(buffer), w0
Prototype
unsigned int __builtin_dmapage(const void *p);
Argument
*p – pointer to DMA address value
Return Value
Returns the page number of a variable located in DMA memory.
Assembler Operator/ Machine Instruction
dmapage
Error Messages
An error message will be displayed if the parameter is not the address of a global symbol.