28.2.56 __builtin_sftac
Description
Shifts accumulator by shift. The valid shift range is -16 to 16.
For example:
volatile register int result asm(“A”);
int i;
result = __builtin_sftac(result,i);
Might generate:
sftac A, w0
Prototype
int __builtin_sftac(int Accum, int shift);
Argument
Accum – Accumulator to shift.
shift – Amount to shift.
Return Value
Returns the shifted result to an accumulator.
Assembler Operator/ Machine Instruction
sftac
Error Messages
An error message will be displayed if:
- the result is not an accumulator register
- Accum is not an accumulator register
- the shift value is not a literal within range