28.2.36 __builtin_mpyn
Description
Computes -a x b ; also prefetches data
ready for a future MAC operation.
xptr may be null to signify no X prefetch to be performed, in
which case the values of xincr and xval
are ignored, but required.
yptr may be null to signify no Y prefetch to be performed, in
which case the values of yincr and yval
are ignored, but required.
xval and yval nominate the address of a C
variable where the prefetched value will be stored.
xincr and yincr may be the literal
values: -6, -4, -2, 0, 2, 4, 6 or an integer value.
For example:
volatile register int result asm("A");
int *xmemory;
int *ymemory;
int xVal, yVal;
result = __builtin_mpy(xVal, yVal,
&xmemory, &xVal, 2,
&ymemory, &yVal, 2);
might generate:
mpy.n w4*w5, A, [w8]+=2, w4, [w10]+=2, w5
Prototype
int __builtin_mpyn(int a, int b,
int **xptr, int *xval, int xincr,
int **yptr, int *yval, int yincr);
Argument
a – Integer multiplicand.
b – Integer multiplier.
xptr – Integer pointer to pointer to x prefetch.
xval – Integer pointer to value of x prefetch.
xincr – Integer increment value of x prefetch.
yptr – Integer pointer to pointer to y prefetch.
yval – Integer pointer to value of y prefetch.
yincr – Integer increment value of y prefetch.
AWB – Integer pointer to accumulator selection.
Return Value
Returns the value of -a x b.
Assembler Operator/ Machine Instruction
mpyn
Error Messages
An error message will be displayed if:
- the result is not an accumulator register
xvalis a null value butxptris not nullyvalis a null value butyptris not null