28.2.16 __builtin_divud
Description
Computes the quotient num / den. A math
error exception occurs if den is zero. Function arguments are
unsigned, as is the function result. The command-line option
-Wconversions can be used to detect unexpected sign conversions.
Prototype
unsigned int __builtin_divud(const unsigned long num, const unsigned int den);
Argument
num – numerator
den – denominator
Return Value
Returns the unsigned integer value of the quotient num /
den.
Assembler Operator/ Machine Instruction
div.ud