28.2.51 __builtin_sacd
Description
Shifts value by shift and returns the value. For example:
volatile register int value asm("A");
int result;
result = __builtin_sacd(value,3);
Might generate:
sacd A, #3, w0
Prototype
int __builtin_sacd(int value, int shift);
Argument
value – Integer number to be shifted.
shift – Literal amount to shift between -16 and 15
Return Value
Returns the shifted result.
Assembler Operator/ Machine Instruction
sacd
Error Messages
An error message will be displayed if:
- the result is not an accumulator register
- the shift value is not a literal within range