28.2.50 __builtin_sac
Description
Shifts a value by shift and returns the value. For example:
volatile register int value asm("A");
long result;
result = __builtin_sac(value,3);
Prototype
long __builtin_sac(int value, int shift);
Argument
value – Integer number to be shifted.
shift – Literal amount to shift between -8 and 7
Return Value
Returns the shifted result.
Assembler Operator/ Machine Instruction
None
Error Messages
An error message will be displayed if: the result is not an accumulator register the shift value is not a literal within range