BLE_GAP_CreateConnParams_T

C

typedef struct BLE_GAP_CreateConnParams_T
{
    uint16_t                scanInterval;
    uint16_t                scanWindow;
    uint8_t                 filterPolicy;
    BLE_GAP_Addr_T          peerAddr;
    BLE_GAP_ConnParams_T    connParams;
} BLE_GAP_CreateConnParams_T;

Description

Structure for configuring parameters to create a BLE connection.

Field Documentation

FieldDescription
scanIntervalScan interval used during connection establishment (0.625 ms units). See Scan interval.
scanWindowScan window used during connection establishment (0.625 ms units). Must be less than or equal to scanInterval. See Scan window.
filterPolicyInitiator filter policy used to determine if the Filter Accept List is used. See Initiator filter policies for possible values. If the Filter Accept List is not used, the peerAddr argument specifies the address type and address of the advertising device to connect to.
peerAddrAddress of the peer device to connect to. Ignored if filterPolicy is set to use the Filter Accept List.
connParamsDesired connection parameters. See BLE_GAP_ConnParams_T for structure details.