4.1.2 Interrupt and Trap Vectors
All dsPIC33CK256MC006 family
devices reserve the addresses between 0x000000 and 0x000200 for hard-coded program
execution vectors. A hardware Reset vector is provided to redirect code execution from
the default value of the PC on device Reset to the actual start of code. A
GOTO instruction is programmed by the user application at address
0x000000 of Flash memory, with the actual address for the start of code at address
0x000002 of Flash memory.
A more detailed discussion of the Interrupt Vector Tables (IVTs) is provided in the Interrupt Controller section.