5.4.6.2 Performing Fault Injection
The following sequence should be followed to inject Faults.
1. Load the data RAM target address into ECCFADDR register.
2. Select the first Fault bit determined by ECCFPTRbits.FLT1PTR[5:0]. The data RAM target bit is inverted to create the Fault.
3. If a double Fault is desired, select the second Fault bit determined by ECCFPTRbits.FLT2PTR[5:0], otherwise set ECCFPTR.FLT2PTR[5:0] = 6'h3F.
4. Perform a read of the data RAM target address.
The ECCSTAT is updated whenever a read occurs and the read address matches ECCFADDR. The read address is the relative address from the start address of the X or Y data spaces. The expected usage of data read Fault injection is to attempt to read a predefined data set with known good ECC and inject an error immediately prior to the ECC evaluation, thereby testing the response of the ECC block under different data stimuli.