1.2.5.61 ADP_NON_VOLATILE_DATA_IND_CALLBACK Typedef
C
typedef void (*ADP_NON_VOLATILE_DATA_IND_CALLBACK)(ADP_NON_VOLATILE_DATA_IND_PARAMS* pNonVolatileDataInd);
Summary
Pointer to a Non-Volatile Data Indication Event handler function.
Description
This data type defines the required function signature for the ADP Non-Volatile Data Indication event handling callback function. The ADP Non-Volatile Data Indication primitive allows the next higher layer to be notified when non-volatile stored data must be updated to be able to restore it after a reset or power cycle of the device. A client must register a pointer using the event handling function whose function signature (parameter and return value types) matches the types specified by this function pointer in order to receive Non-Volatile Data Indication events back from module.
Parameters
| Param | Description |
|---|---|
| pNonVolatileDataInd | Pointer to structure containing the Non Volatile data. See ADP_NON_VOLATILE_DATA_IND_PARAMS. |
Returns
None.
Example
App_NonVolatileDataIndication(ADP_NON_VOLATILE_DATA_IND_PARAMS *params)
{
// Store non-volatile data
}
Remarks
None.