1.2.5.32 ADP_GET_CFM_CALLBACK Typedef
C
typedef void (*ADP_GET_CFM_CALLBACK)(ADP_GET_CFM_PARAMS* pGetCfm);
Summary
Pointer to a Get Confirm Event handler function.
Description
This data type defines the required function signature for the ADP Get Confirm event handling callback function. The ADP Get Confirm primitive allows the upper layer to be notified of the completion of an ADP Get Request. A client must register a pointer using the event handling function whose function signature (parameter and return value types) matches the types specified by this function pointer in order to receive Get Confirm events back from module.
The Get Confirm is generated after ADP_GetRequest function call to indicate the result.
Parameters
| Param | Description |
|---|---|
| pGetCfm | Pointer to structure containing the Get result. See ADP_GET_CFM_PARAMS. |
Returns
None.
Example
App_GetConfirm(ADP_GET_CFM_PARAMS *params)
{
// Check result
if (params->status == G3_SUCCESS)
{
// The value is in params->attributeValue
}
}
Remarks
None.