1.2.5.34 ADP_MacGetRequest Function
C
void ADP_MacGetRequest (
uint32_t attributeId,
uint16_t attributeIndex
);
Summary
This primitive gets the value of an attribute from the MAC information base.
Description
The ADP MAC Get Request primitive allows the upper layer to get the value of an attribute from the MAC information base. The upper layer cannot access directly the MAC layer while ADP is running. Result is provided in the corresponding ADP MAC Get Confirm callback.
Parameters
| Param | Description |
|---|---|
| attributeId | The identifier of the MAC IB attribute to read. See MAC_WRP_PIB_ATTRIBUTE. |
| attributeIndex | The index within the table of the specified IB attribute to read. |
Returns
None.
Example
ADP_MacGetRequest(MAC_WRP_PIB_SHORT_ADDRESS, 0);
// Wait for MAC Get Confirm
Remarks
None.