1.2.5.81 LBP_SET_PARAM_CONFIRM Struct

C

typedef struct
{
    /* The identifier of the IB attribute to set */
    uint32_t attributeId;
    /* The index within the table of the specified IB attribute */
    uint16_t attributeIndex;
    /* The result of the set request */
    LBP_STATUS status;
} LBP_SET_PARAM_CONFIRM;

Summary

Defines the parameters for the result of setting a LBP parameter.

Description

The structure contains the result of setting a LBP parameter.

Field description:

  • attributeId: The identifier of the IB attribute to set.
  • attributeIndex: The index within the table of the specified IB attribute.
  • status: The result of the set request. See LBP_STATUS.

Remarks

None.