1.2.5.25 ADP_PAN_DESCRIPTOR Struct

C

typedef struct
{
    /* The 16-bit PAN identifier */
    uint16_t panId;
    /* The 16 bit short address of a device in this PAN to be used as the LBA
     * by the associating device */
    uint16_t lbaAddress;
    /* The estimated route cost from LBA to the coordinator */
    uint16_t rcCoord;
    /* The 8-bit link quality of LBA */
    uint8_t linkQuality;
    /* The media type (PLC or RF) used to communicate with LBA */
    uint8_t mediaType;
} ADP_PAN_DESCRIPTOR;

Summary

Defines the structure of a PAN Descriptor.

Description

This data type defines the structure of a PAN Descriptor. It used in ADP Discovery Indication to store the parameters of the discovered PAN.

Field description:

  • panId: The 16-bit PAN identifier
  • lbaAddress: The 16 bit short address of a device in this PAN to be used as the LBA (LoWPAN Bootstrap Agent) by the associating device
  • rcCoord: The estimated route cost from LBA to the PAN Coordinator
  • linkQuality: The Link Quality measured when receiving frames from the LBA
  • mediaType: The media type (PLC or RF) on which the frame from LBA was received

Remarks

None.