1.2.5.37 ADP_MAC_GET_CFM_PARAMS Struct

C

typedef struct
{
    /* The identifier of the IB attribute read */
    uint32_t attributeId;
    /* The index within the table of the specified IB attribute read */
    uint16_t attributeIndex;
    /* The status of the get request */
    uint8_t status;
    /* The length of the value of the attribute read from the IB */
    uint8_t attributeLength;
    /* The value of the attribute read from the IB */
    uint8_t attributeValue[144];
} ADP_MAC_GET_CFM_PARAMS;

Description

This data type defines the structure of an ADP MAC Get Confirm callback. It is returned by the ADP_MAC_GET_CFM_CALLBACK function to indicate the Get result and value.

Field description:

  • attributeId: The identifier of the IB attribute to get. See MAC_WRP_PIB_ATTRIBUTE.
  • attributeIndex: The index within the table of the specified IB attribute.
  • status: The result of the get request.
  • attributeLength: The length of the value of the attribute read from the IB.
  • attributeValue: Array containing the value of the attribute read from the IB.

Remarks

None.