1.2.5.42 ADP_MacSetRequest Function
C
void ADP_MacSetRequest (
uint32_t attributeId,
uint16_t attributeIndex,
uint8_t attributeLength,
const uint8_t *pAttributeValue
);
Summary
This primitive sets the value of an attribute in the MAC information base.
Description
The ADP MAC Set Request primitive allows the upper layer to set the value of an attribute in the MAC information base. The upper layer cannot access directly the MAC layer while ADP is running. Result is provided in the corresponding ADP MAC Set Confirm callback.
Parameters
| Param | Description |
|---|---|
| attributeId | The identifier of the MAC IB attribute to read. See MAC_WRP_PIB_ATTRIBUTE. |
| attributeIndex | The index within the table of the specified IB attribute to read |
| attributeLength | The length of the value of the attribute to set |
| pAttributeValue | Pointer to the value of the attribute to set |
Returns
None.
Example
uint8_t pAttributeValue[144]; pAttributeValue[0] = 5; ADP_MacSetRequest(MAC_WRP_PIB_MAX_BE, 0, 1, pAttributeValue); // Wait for MAC Set Confirm
Remarks
None.