24.2.1.3 Step 3
Select either or both check boxes as required. If MSS DDR is selected, the FIC_2 Configurator shows the graphical illustration of the connectivity between the FIC_2 APB master and MSS DDR APB slave through CoreSF2Config, as shown in the following figure.
CoreSF2Config must be instantiated in SmartDesign.connections made as illustrated in FIC_2 configurator. The following figure shows the connectivity between APB configuration interfaces of the SERDES and DDR subsystems (both are selected).
If System Builder is used for creating the design, CoreSF2Config is instantiated and connections are made automatically.