31.8.14 ETH Interrupt Status Register
This register indicates the source of the interrupt. An interrupt source must be enabled in the mask register first so the corresponding bits of this register will be set and the ETH interrupt signal will be asserted in the system.
Symbol | Description | Symbol | Description | Symbol | Description |
---|---|---|---|---|---|
R | Readable bit | HC | Cleared by Hardware | (Grey cell) | Unimplemented |
W | Writable bit | HS | Set by Hardware | X | Bit is unknown at Reset |
K | Write to clear | S | Software settable bit | — | — |
Name: | ISR |
Offset: | 0x1024 |
Reset: | 0x00000000 |
Property: | Write to Clear |
Bit | 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | |
TSUTIMCMP | WOL | RXLPISBC | SRI | PDRSFT | PDRQFT | ||||
Access | R | R | R | R | R | R | |||
Reset | 0 | 0 | 0 | 0 | 0 | 0 |
Bit | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | |
PDRSFR | PDRQFR | SFT | DRQFT | SFR | DRQFR | ||||
Access | R | R | R | R | R | R | |||
Reset | 0 | 0 | 0 | 0 | 0 | 0 |
Bit | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | |
PFTR | PTZ | PFNZ | HRESP | ROVR | |||||
Access | R | R | R | R | R | ||||
Reset | 0 | 0 | 0 | 0 | 0 |
Bit | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 | |
TCOMP | TFC | RLEX | TUR | TXUBR | RXUBR | RCOMP | MFS | ||
Access | R | R | R | R | R | R | R | R | |
Reset | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 |
Bit 29 – TSUTIMCMP TSU Timer Comparison
Indicates when TSU timer count value is equal to programmed value.
Cleared on read.
Bit 28 – WOL Wake On LAN
WOL interrupt. Indicates a WOL message has been received.
Bit 27 – RXLPISBC Receive LPI indication Status Bit Change
Receive LPI indication status bit change.
Cleared on read.
Bit 26 – SRI TSU Seconds Register Increment
Indicates the register has incremented.
Cleared on read.
Bit 25 – PDRSFT PDelay Response Frame Transmitted
Indicates a PTP pdelay_resp frame has been transmitted.
Cleared on read.
Bit 24 – PDRQFT PDelay Request Frame Transmitted
Indicates a PTP pdelay_req frame has been transmitted.
Cleared on read.
Bit 23 – PDRSFR PDelay Response Frame Received
Indicates a PTP pdelay_resp frame has been received.
Cleared on read.
Bit 22 – PDRQFR PDelay Request Frame Received
Indicates a PTP pdelay_req frame has been received.
Cleared on read.
Bit 21 – SFT PTP Sync Frame Transmitted
Indicates a PTP sync frame has been transmitted.
Cleared on read.
Bit 20 – DRQFT PTP Delay Request Frame Transmitted
Indicates a PTP delay_req frame has been transmitted.
Cleared on read.
Bit 19 – SFR PTP Sync Frame Received
Indicates a PTP sync frame has been received.
Cleared on read.
Bit 18 – DRQFR PTP Delay Request Frame Received
Indicates a PTP delay_req frame has been received.
Cleared on read.
Bit 14 – PFTR Pause Frame Transmitted
Indicates a pause frame has been successfully transmitted after being initiated from the Network Control Register.
Cleared on read.
Bit 13 – PTZ Pause Time Zero
Set when either the Pause Time Register at address 0x1038 decrements to zero, or when a valid pause frame is received with a zero pause quantum field.
Cleared on read.
Bit 12 – PFNZ Pause Frame with Non-zero Pause Quantum Received
Indicates a valid pause has been received that has a non-zero pause quantum field.
Cleared on read.
Bit 11 – HRESP HRESP Not OK
Set when the DMA block sees HRESP not OK.
Cleared on read.
Bit 10 – ROVR Receive Overrun
Set when the receive overrun status bit is set.
Cleared on read.
Bit 7 – TCOMP Transmit Complete
Set when a frame has been transmitted.
Cleared on read.
Bit 6 – TFC Transmit Frame Corruption Due to AXI Error
Transmit frame corruption due to AXI error. Set if an error occurs during reading a transmit frame from the AXI, including HRESP errors and buffers exhausted mid frame.
Bit 5 – RLEX Retry Limit Exceeded
Retry Limit Exceeded Transmit error.
Cleared on read.
Bit 4 – TUR Transmit Underrun
This interrupt is set if the transmitter was forced to terminate an ongoing frame transmission due to further data being unavailable.
This interrupt is also set if a transmitter status write back has not completed when another status write back is attempted.
This interrupt is also set when the transmit DMA has written the SOP data into the FIFO and either the AXI bus was not granted in time for further data, or because an AXI not OK response was returned, or because the used bit was read.
Bit 3 – TXUBR TX Used Bit Read
Set when a transmit buffer descriptor is read with its used bit set.
Cleared on read.
Bit 2 – RXUBR RX Used Bit Read
Set when a receive buffer descriptor is read with its used bit set.
Cleared on read.
Bit 1 – RCOMP Receive Complete
A frame has been stored in memory.
Cleared on read.
Bit 0 – MFS Management Frame Sent
The PHY Maintenance Register has completed its operation.
Cleared on read.