2.63.12 MCSPIx_ErrorGet Function
C
/* x = MCSPI instance number */
/* MCSPI slave mode */
MCSPI_SLAVE_ERROR MCSPIx_ErrorGet(void)
Summary
Returns the status of MCSPI transfer
Description
This function returns the error status of the last MCSPI transfer. Applicaiton must check the status of a transfer in the application callback and take appropriate action in case there is an error during the data transfer. Calling this API clears the error status flags.
Precondition
The MCSPIx_Initialize() should have been called.
Parameters
None.
Returns
MCSPI_SLAVE_ERROR - MCSPI Slave Errors
Example
void MCSPIEventHandler(uintptr_t context ) { if (MCSPI1_ErrorGet() == MCSPI_SLAVE_ERROR_NONE) { nBytesAvailable = MCSPI1_ReadCountGet(); nBytesRead = MCSPI1_Read(APP_RxData, nBytesAvailable); } else { // Handle error } } MCSPI1_CallbackRegister(MCSPIEventHandler, (uintptr_t) 0);
Remarks
None.