2.63.8 MCSPIx_IsTransmitterBusy Function
C
/* x = MCSPI instance number */ /* MCSPI master (blocking) mode */ bool MCSPIx_IsTransmitterBusy (void):
Summary
Returns transfer status of MCSPI
Description
MCSPI master mode
In master mode, this function returns true if the MCSPI module is busy with a transfer. The application can use the function to check if MCSPI module is busy before calling any of the data transfer functions.
Precondition
The MCSPIx_Initialize() should have been called once. The module should have been configured for interrupt mode operation in MCC.
Parameters
None.
Returns
Param | Description |
---|---|
true | Transfer is currently in progress (in master mode) |
false | Transfer is completed (in master mode) |
Example
MCSPI master (blocking mode)
// The following code example demonstrates the use of the // MCSPIx_IsTransmitterBusy() function. This example shows a blocking while // loop. uint8_t dataBuffer[20]; MCSPI1_Initialize(); while (MCSPI1_IsTransmitterBusy() == true) { // Wait here till the transfer is done. } MCSPI1_Write(dataBuffer, 20);
Remarks
None