2.115.4 TIMER32_x_PreLoadCountSet Function

C

/* x = Timer32 instance number */

void TIMER32_x_PreLoadCountSet(uint32_t count)

Summary

Sets the timer pre-load value

Description

Sets the timer pre-load value. This is used by H/W when the counter is to be restarted automatically; this will become the new value of the counter upon restart.

Precondition

TIMER32_x_Initialize() function must have been called first and auto-restart must be enabled

Parameters

ParamDescription
counttimer pre-load value

Returns

None

Example

TIMER32_0_PreLoadCountSet(1000);

Remarks

None