2.115.9 TIMER32_x_FrequencyGet Function

C

/* x = Timer32 instance number */

uint32_t TIMER32_x_FrequencyGet(void)

Summary

Returns the input frequency of the Timer32 peripheral

Description

Returns the input frequency of the Timer32 peripheral

Precondition

TIMER32_x_Initialize() function must have been called first.

Parameters

None

Returns

Input frequency of the Timer32 peripheral

Example

uint32_t freq = TIMER32_0_FrequencyGet();

Remarks

None