2.115.15 TMR32_CALLBACK Typedef

C

typedef void (*TMR32_CALLBACK)(uintptr_t context);

Summary

Defines the data type and function signature for the timer peripheral callback function.

Description

This data type defines the function signature for the timer peripheral callback function. The timer peripheral will call back the client's function with this signature when the timer expires.

Precondition

TIMER32_x_Initialize() function must have been called first.

Parameters

ParamDescription
contextA value (usually a pointer) which is passed (unused) into the function identified by the callback parameter

Returns

None

Example

void tmr32_callback(uint32_t status, uintptr_t context)
{
    /* Timer expired */
}

TIMER32_0_CallbackRegister(tmr32_callback, 0);

Remarks

None