2.29.6 DMA_ChannelEnable Function

C

void DMA_ChannelEnable ( DMA_CHANNEL channel )

Summary

The function enables the specified DMA channel.

Description

The function enables the specified DMA channel. Once enabled, DMA will initiate a block transfer when the selected trigger is received

Precondition

DMA should have been initialized by calling DMA_Initialize.

Parameters

ParamDescription
channelThe DMA channel that needs to be disabled

Returns

None.

Example

// Enable the channel.
DMA_ChannelEnable (DMA_CHANNEL_0);

Remarks

None.