2.29.5 DMA_ChannelDisable Function

C

void DMA_ChannelDisable ( DMA_CHANNEL channel )

Summary

The function disables the specified DMA channel.

Description

The function disables the specified DMA channel. Once disabled, the channel will ignore triggers and will not transfer data till the next time a DMA_ChannelTransfer function is called. If there is a transfer already in progress, this will suspended.

Precondition

DMA should have been initialized by calling DMA_Initialize.

Parameters

ParamDescription
channelThe DMA channel that needs to be disabled

Returns

None.

Example

// Disable the channel.
DMA_ChannelDisable (DMA_CHANNEL_0);

Remarks

None.