21.14.67.1 Arguments

filename

Specifies the name and destination of the timing report.

-type timing

Specifies the type of report to generate.

−print_summary value

Specifies whether to print the summary section in the timing report.

Table 21-34. Values
ValueDescription

yes

Includes summary section in the timing report (the default value).

no

Excludes summary section in the timing report

−analysis value

Specifies whether the report will consider minimum analysis or maximum analysis.

Table 21-35. Values
ValueDescription

min

Timing report considers minimum analysis

max

Timing report considers maximum analysis (the default value)

−use_slack_threshold value

Specifies whether the report will consider slack threshold.

Table 21-36. Values
ValueDescription

yes

Includes slack threshold in the timing report.

no

Excludes slack threshold in the timing report (the default value)

−slack_threshold value

Specifies the threshold to consider when reporting path slacks. This is a floating-point number in nanoseconds (ns). By default, there is no threshold (all slacks are reported).

−print_paths value

Specifies whether the path section (clock domains and in-to-out paths) will be printed in the timing report.

Table 21-37. Values
ValueDescription

yes

Includes path section in the timing report (the default value)

no

Excludes path sections from the timing report

−max_paths value

Defines the maximum number of paths to display for each set. This is a positive integer value greater than zero. The default is 5.

−max_expanded_paths value

Defines the number of paths to expand per set. This is a positive integer value greater than zero. The default is 1.

−include_user_sets value

Defines whether to include the user defined sets in the timing report.

Table 21-38. Values
ValueDescription

yes

Includes user defined sets in the timing report (the default value)

no

Excludes user defined sets from the timing report

−include_pin_to_pin value

Specifies whether to show pin-to-pin paths in the timing report.

Table 21-39. Values
ValueDescription

yes

Includes pin-to-pin paths in the timing report (the default value).

no

Excludes pin-to-pin paths from the timing report

−include_clock_domains value

Defines whether to include clock domains in the timing report.

Table 21-40. Values
ValueDescription

yes

Includes clock domains

no

Excludes clock domains from the timing report

−select_clock_domains value

Specifies whether to show the clock domain list in the timing report.

Table 21-41. Values
ValueDescription

yes

Includes the clock domain list in the timing report

no

Excludes the clock domain list from the timing report (the default value)

−clock_domain clock_domain_list

Defines the clock domain to be considered in the clock domain section. The domain list is a series of strings with domain names separated by spaces. Both the summary and the path sections in the timing report display only the listed clock domains.

−format value

Specifies the output format of the generated the report.

Table 21-42. Values
ValueDescription

text

Generates a text report; text is the default value

csv

Generates the report in a comma-separated value format which you can import into a spreadsheet